Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static AssemblyDrawingBuilder.DrawingTypes |
AssemblyDrawingBuilder.DrawingTypes.MASTER_MODEL |
static AssemblyDrawingBuilder.DrawingTypes |
AssemblyDrawingBuilder.DrawingTypes.SELF_CONTAINED |
Modifier and Type | Method and Description |
---|---|
AssemblyDrawingBuilder.DrawingTypes |
AssemblyDrawingBuilder.enumDrawingType()
Returns the option for the assembly drawing operation
License requirements: None. |
static AssemblyDrawingBuilder.DrawingTypes |
AssemblyDrawingBuilder.DrawingTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssemblyDrawingBuilder.DrawingTypes |
AssemblyDrawingBuilder.DrawingTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssemblyDrawingBuilder.DrawingTypes[] |
AssemblyDrawingBuilder.DrawingTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssemblyDrawingBuilder.setEnumDrawingType(AssemblyDrawingBuilder.DrawingTypes enumDrawingType)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.