Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static CreateBoxBuilder.BoxType |
CreateBoxBuilder.BoxType.BOUNDING
bounding box
|
static CreateBoxBuilder.BoxType |
CreateBoxBuilder.BoxType.GENERAL
general box
|
Modifier and Type | Method and Description |
---|---|
CreateBoxBuilder.BoxType |
CreateBoxBuilder.type()
Returns the box type.
|
static CreateBoxBuilder.BoxType |
CreateBoxBuilder.BoxType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CreateBoxBuilder.BoxType |
CreateBoxBuilder.BoxType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CreateBoxBuilder.BoxType[] |
CreateBoxBuilder.BoxType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CreateBoxBuilder.setType(CreateBoxBuilder.BoxType type)
License requirements: ug_mold_design ("UG MOLD") OR nx_electrode_wizard ("NX Electrode Wizard") OR prog_die_wizard ("UG/Progressive Die Wizard") OR studio_free_form ("STUDIO FREE FORM") OR features_modeling ("FEATURES MODELING") OR solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.