Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.BILATERAL_TOLERANCE |
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.EQUAL_BILATERAL_TOLERANCE |
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.NO_TOLERANCE |
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.UNILATERAL_MINUS |
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.UNILATERAL_PLUS |
Modifier and Type | Method and Description |
---|---|
AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.tolerance()
Returns the tolerance type
License requirements: None. |
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutoDimensionBuilder.ToleranceType |
AutoDimensionBuilder.ToleranceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutoDimensionBuilder.ToleranceType[] |
AutoDimensionBuilder.ToleranceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AutoDimensionBuilder.setTolerance(AutoDimensionBuilder.ToleranceType toleranceType)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.