Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
DieCavityAndSlugHoleBuilder.ClearanceOptionItems.CONSTANT
The design option is normal
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
DieCavityAndSlugHoleBuilder.ClearanceOptionItems.VARIABLE
The design option is fineblanking
|
Modifier and Type | Method and Description |
---|---|
DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
DieCavityAndSlugHoleBuilder.normalClearanceOption()
Returns the normal clearance option
License requirements: None. |
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
DieCavityAndSlugHoleBuilder.ClearanceOptionItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
DieCavityAndSlugHoleBuilder.ClearanceOptionItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.ClearanceOptionItems[] |
DieCavityAndSlugHoleBuilder.ClearanceOptionItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieCavityAndSlugHoleBuilder.setNormalClearanceOption(DieCavityAndSlugHoleBuilder.ClearanceOptionItems normalClearanceOption)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.