Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ObjectAttributeManagementBuilder.ShowType |
ObjectAttributeManagementBuilder.ShowType.SHOW_ATTRIBUTE_OF_SELECTED_OBJECT |
static ObjectAttributeManagementBuilder.ShowType |
ObjectAttributeManagementBuilder.ShowType.SHOW_OBJECT_ACCORDING_TO_ATTRIBUTE |
Modifier and Type | Method and Description |
---|---|
ObjectAttributeManagementBuilder.ShowType |
ObjectAttributeManagementBuilder.type()
Returns the type show objects or attributes
License requirements: None. |
static ObjectAttributeManagementBuilder.ShowType |
ObjectAttributeManagementBuilder.ShowType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ObjectAttributeManagementBuilder.ShowType |
ObjectAttributeManagementBuilder.ShowType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ObjectAttributeManagementBuilder.ShowType[] |
ObjectAttributeManagementBuilder.ShowType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ObjectAttributeManagementBuilder.setType(ObjectAttributeManagementBuilder.ShowType type)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.