Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static SpecialFormingBuilder.BlockType |
SpecialFormingBuilder.BlockType.BOUNDED_BLOCK |
static SpecialFormingBuilder.BlockType |
SpecialFormingBuilder.BlockType.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
SpecialFormingBuilder.BlockType |
SpecialFormingBuilder.boundedBlockOrUserDefined()
Returns the bounded block or user defined
License requirements: None. |
static SpecialFormingBuilder.BlockType |
SpecialFormingBuilder.BlockType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpecialFormingBuilder.BlockType |
SpecialFormingBuilder.BlockType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpecialFormingBuilder.BlockType[] |
SpecialFormingBuilder.BlockType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpecialFormingBuilder.setBoundedBlockOrUserDefined(SpecialFormingBuilder.BlockType boundedBlockOrUserDefined)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.