Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static AutoDimensionBuilder.MainType |
AutoDimensionBuilder.MainType.CREATE_ORDINATE_DIMENSION |
static AutoDimensionBuilder.MainType |
AutoDimensionBuilder.MainType.EDIT_ORDINATE_DIMENSION |
Modifier and Type | Method and Description |
---|---|
AutoDimensionBuilder.MainType |
AutoDimensionBuilder.type()
Returns the type create or edit ordinate dimension
License requirements: None. |
static AutoDimensionBuilder.MainType |
AutoDimensionBuilder.MainType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutoDimensionBuilder.MainType |
AutoDimensionBuilder.MainType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutoDimensionBuilder.MainType[] |
AutoDimensionBuilder.MainType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AutoDimensionBuilder.setType(AutoDimensionBuilder.MainType type)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.