Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.CIRCLE
Die shoe slug type is circle
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.CLEARANCE
Die shoe slug type is clearance
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.FILLET
Die shoe slug type is fillet
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.MICKEY
Die shoe slug type is mickey
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.NONE
Die shoe slug type is none
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.RECTANGLE
Die shoe slug type is rectangle
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.SLOT_HOR
Die shoe slug type is slot horizontal
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.SLOT_VER
Die shoe slug type is slot vertical
|
Modifier and Type | Method and Description |
---|---|
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.normalDieShoeSlug()
Returns the normal dsslug
License requirements: None. |
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems[] |
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieCavityAndSlugHoleBuilder.setNormalDieShoeSlug(DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems normalDieShoeSlug)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.