Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static SolidPatchBuilder.SolidPatchType |
SolidPatchBuilder.SolidPatchType.LINK_BODY
Link body type indicates to create link body
|
static SolidPatchBuilder.SolidPatchType |
SolidPatchBuilder.SolidPatchType.SOLID_PATCH
Solid patch type indicates to create solid patch
|
Modifier and Type | Method and Description |
---|---|
SolidPatchBuilder.SolidPatchType |
SolidPatchBuilder.patchType()
Returns the patch type of the solid patch creation.
|
static SolidPatchBuilder.SolidPatchType |
SolidPatchBuilder.SolidPatchType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SolidPatchBuilder.SolidPatchType |
SolidPatchBuilder.SolidPatchType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SolidPatchBuilder.SolidPatchType[] |
SolidPatchBuilder.SolidPatchType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SolidPatchBuilder.setPatchType(SolidPatchBuilder.SolidPatchType patchType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.