Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems.DIE_SIDE
The offset side is die
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems.PUNCH_SIDE
The offset side is punch
|
Modifier and Type | Method and Description |
---|---|
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
DieCavityAndSlugHoleBuilder.normalOffsetSide()
Returns the normal offset side
License requirements: None. |
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems[] |
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieCavityAndSlugHoleBuilder.setNormalOffsetSide(DieCavityAndSlugHoleBuilder.OffsetSideOptionItems normalOffsetSide)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.