public static class DieCavityAndSlugHoleBuilder.OffsetSideOptionItems extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIE_SIDE
The offset side is die
|
static int |
_PUNCH_SIDE
The offset side is punch
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
DIE_SIDE
The offset side is die
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
PUNCH_SIDE
The offset side is punch
|
Modifier and Type | Method and Description |
---|---|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems[] |
values()
Returns an array that contains the values for this enum.
|
public static final DieCavityAndSlugHoleBuilder.OffsetSideOptionItems DIE_SIDE
public static final DieCavityAndSlugHoleBuilder.OffsetSideOptionItems PUNCH_SIDE
public static final int _DIE_SIDE
public static final int _PUNCH_SIDE
public static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems valueOf(int value)
public static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems valueOf(String name)
public static DieCavityAndSlugHoleBuilder.OffsetSideOptionItems[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.