Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.BlankOption |
LsdynaGeometryPreparationBuilder.BlankOption.CURVE
Select several curves to create a blank.
|
static LsdynaGeometryPreparationBuilder.BlankOption |
LsdynaGeometryPreparationBuilder.BlankOption.SHEET
Select a sheet body as blank.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.BlankOption |
LsdynaGeometryPreparationBuilder.blankOptionType()
Returns the blank option.
|
static LsdynaGeometryPreparationBuilder.BlankOption |
LsdynaGeometryPreparationBuilder.BlankOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.BlankOption |
LsdynaGeometryPreparationBuilder.BlankOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.BlankOption[] |
LsdynaGeometryPreparationBuilder.BlankOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setBlankOptionType(LsdynaGeometryPreparationBuilder.BlankOption enumBlankOption)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.