Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.TargetBinder |
LsdynaGeometryPreparationBuilder.TargetBinder.BINDER
For the process, the target of binder is binder.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
LsdynaGeometryPreparationBuilder.TargetBinder.DIE
For the process, the target of binder is die.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
LsdynaGeometryPreparationBuilder.TargetBinder.PUNCH
For the process, the target of binder is punch.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.TargetBinder |
LsdynaGeometryPreparationBuilder.targetBinderType()
Returns the type of binder target.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
LsdynaGeometryPreparationBuilder.TargetBinder.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
LsdynaGeometryPreparationBuilder.TargetBinder.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.TargetBinder[] |
LsdynaGeometryPreparationBuilder.TargetBinder.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setTargetBinderType(LsdynaGeometryPreparationBuilder.TargetBinder enumTargetBinder)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.