AddObjectsToRegionBuilder Class |
Creates the builder for associating the symbols from library to the region |
AddRemoveBoxViewBuilder Class |
This class is used to construct the add remove box view Builder |
AnnotationSettingsBuilder Class |
Represents a Drawings.AnnotationSettingsBuilder . |
AutomationBookletBuilder Class |
Represents a NXOpen.Drawings.AutomationBookletBuilder |
AutomationTemplateRegionBuilder Class |
Represents a NXOpen.Drawings.AutomationTemplateRegionBuilder |
BaseHalfSectionLine Class |
Represents a Base Half Section Line. |
BasePointToPointSectionLine Class |
Represents a Base Point to Point Section Line. |
BaseSteppedSectionLine Class |
Represents a Base Stepped Section Line. |
BaseView Class |
Represents a Base View. |
BaseViewBuilder Class |
Represents a NXOpen.Drawings.BaseView builder |
BaseViewStyle Class |
Represents set of Base View Style Preferences applicable to drafting views. |
BorderAndZoneStyleBuilder Class |
Represents the Border and Zone Style Builder which manages all the style attributes related * to sheet borders, sheet margins and sheet zones. |
BordersAndZones Class |
Represents Borders and Zones |
BordersAndZonesBuilder Class |
Builder for creating Borders and Zones. |
BordersAndZonesCollection Class |
Represents a collection of NXOpen.Drawings.BordersAndZones objects |
BrokenViewBuilder Class |
This class is used to construct the broken view Builder |
CompareReportBuilder Class |
Represents a NXOpen.Drawings.CompareReportBuilder builder |
ConversionProcessSettingsBuilder Class |
Represents a Drawings.ConversionProcessSettingsBuilder . |
ConvertDraftingContentsBuilder Class |
Represents a Drawings.ConvertDraftingContentsBuilder . |
ConvertToPMIBuilderManager Class |
Represents NXOpen.Drawings.ConvertToPMIBuilderManager |
CustomViewSettingsBuilder Class |
this class represents the this class represents Drawings. |
DetailView Class |
Represents a Detail View. |
DetailViewBuilder Class |
Represents a NXOpen.Drawings.DetailView . |
DraftingBody Class |
Represents a drafting body. |
DraftingBodyCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.DraftingBody`s. |
DraftingComponentSelectionBuilder Class |
This builder allows the user to select a view in which component objects can be designated as primary or secondary geometry |
DraftingCurve Class |
Represents a Drafting VD Curve. |
DraftingCurveCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.DraftingCurve`s. |
DraftingCurveInfo Class |
Represents Drafting Curve Info |
DraftingView Class |
Represents a drafting view. |
DraftingViewCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.DraftingView`s. |
DrawingCompareSettingsBuilder Class |
Represents a NXOpen.Drawings.DrawingCompareSettingsBuilder builder |
DrawingFormatSheetBuilder Class |
Represents a NXOpen.Drawings.DrawingFormatSheetBuilder |
DrawingRegion Class |
Represents a Drawing Region |
DrawingRegionBuilder Class |
Represents a Drawing Region Builder |
DrawingRegionCollection Class |
Represents a collection of drawing regions |
DrawingRegionRulesBuilder Class |
Represents a Drawing region rules builder |
DrawingSheet Class |
Represents a drawing sheet. |
DrawingSheetBuilder Class |
Represents a NXOpen.Drawings.DrawingSheetBuilder |
DrawingSheetCollection Class |
Represents a collection of drawing sheets. |
DrawingView Class |
Drawing View - an empty view created without any geometric objects. |
DrawingViewBuilder Class |
This builder allows the user to create a Drawing View |
DrawingsPropertiesBuilder Class |
Represents an NXOpen.Drawings.DrawingsPropertiesBuilder to be used for marking the component as secondary geometry. |
EditSectionLineSettingsBuilder Class |
Represents a NXOpen.Drawings.EditSectionLineSettingsBuilder builder. |
EditViewLabelSettingsBuilder Class |
Represents a NXOpen.Drawings.EditViewLabelSettingsBuilder builder. |
EditViewSettingsBuilder Class |
Represents a NXOpen.Drawings.EditViewSettingsBuilder builder. |
FlatPatternObject Class |
Provides an interface to the data available for flat pattern objects on drawing views. |
FlatPatternViewStyle Class |
Provides access to object and callout properties for sheet-metal data in flat pattern views on drawings. |
GeneralViewStyle Class |
Represents set of General View Styles Preferences applicable to drafting views. |
GeneralWorkFlowBuilder Class |
Represents a NXOpen.Drawings.GeneralWorkFlowBuilder |
HalfPictorialSectionLine Class |
Half Pictorial Section Line is used to create a pictorial view with half of the part sectioned and the other half un-sectioned. |
HalfSectionLine Class |
Half Section Line is used to create a view with half of the part sectioned and the other half un-sectioned. |
HalfSectionLineBuilder Class |
Represents a NXOpen.Drawings.HalfSectionLineBuilder . |
HiddenLinesViewStyle Class |
Represents set of Hidden Lines View Style Preferences applicable to drafting views. |
HiddenObjectsBuilder Class |
This builder allows the user to select a view in which component objects can be designated as hidden or shown |
HingeLineBuilder Class |
Represents a Drawings. |
InheritPmiViewStyle Class |
Represents set of InheritPmiViewStyle applicable to drafting views. |
MarkAsTemplateBuilder Class |
Represents a NXOpen.Drawings.MarkAsTemplateBuilder |
MultipleViewPlacementBuilder Class |
This builder allows the user to create a Multiple View Placement |
OrderManager Class |
Represents an object that manages orders. |
OrientationViewStyle Class |
Represents set of Orientation View Style Preferences applicable to drafting views. |
OrientedSectionLine Class |
Represents a Oriented Section Line. |
OrientedSectionLineBuilder Class |
Represents a NXOpen.Drawings.OrientedSectionLineBuilder . |
OvtBuilder Class |
Represents a NXOpen.Drawings.OvtBuilder |
ParentViewBuilder Class |
Represents a NXOpen.Drawings.ParentViewBuilder . |
PerspectiveViewStyle Class |
Represents set of PerspectiveViewStyle applicable to drafting views. |
PictorialSectionLine Class |
A Pictorial Simple or Pictorial Stepped Section Line. |
PointAndAngleSectionLine Class |
Point and Angle Section Line lets you create a view with multiple segment cuts with no bends. |
PointAndAngleSectionLineBuilder Class |
Represents a NXOpen.Drawings.PointAndAngleSectionLineBuilder . |
PointToPointSectionLine Class |
Point to Point Section Line lets you create a view with multiple segment cuts with no bends. |
PointToPointSectionLineBuilder Class |
Represents a NXOpen.Drawings.PointToPointSectionLineBuilder . |
ProjectedView Class |
Represents a Projected View. |
ProjectedViewBuilder Class |
Represents a NXOpen.Drawings.ProjectedView builder |
ProjectedViewOrientationBuilder Class |
Represents a NXOpen.Drawings.ProjectedViewOrientationBuilder |
ProjectedViewStyle Class |
Represents set of Projected View Style Preferences applicable to drafting views. |
RefineDisplayBuilder Class |
Represents a NXOpen.Drawings.RefineDisplayBuilder . |
RemoveObjectsBuilder Class |
Creates the builder for removing associated objects from the region |
RenderSet Class |
Represents a RenderSet. |
ReportBuilder Class |
Represents a Drawings.ReportBuilder . |
RevolvedSectionLine Class |
Revolved Section Line is used to create section views which are revolved about an axis. |
RevolvedSectionLineBuilder Class |
Represents a NXOpen.Drawings.RevolvedSectionLineBuilder . |
SecondaryGeometryInViewsBuilder Class |
This builder allows the user to select existing view(s) in which component objects can be designated as secondary or primary |
SectionInViewBuilder Class |
This builder allows the user to select a view in which component or solid body objects can be designated as section, non-sectioned, or neither |
SectionLine Class |
Represents a Section Line. |
SectionLineBuilder Class |
Represents a NXOpen.Drawings.SectionLineBuilder . |
SectionLineCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.SectionLine`s. |
SectionLineSegmentBuilder Class |
Represents a NXOpen.Drawings.SectionLineSegmentBuilder . |
SectionLineSegmentBuilderList Class |
Represents a list of objects. |
SectionLineSegmentPointBuilder Class |
Represents Section Line Segment Point Builder |
SectionLineSegmentPointListBuilder Class |
Represents SectionLineSegmentPointListBuilder class. |
SectionLineSegmentsBuilder Class |
Represents a class Drawings. |
SectionLineSettingsBuilder Class |
Represents the Section Line Settings Builder (Drawings. |
SectionLineStyleBuilder Class |
Represents a Drawings. |
SectionView Class |
Represents a Section View. |
SectionViewBuilder Class |
Represents a NXOpen.Drawings.SectionView builder |
SectionViewStyle Class |
Represents set of Section View Style Preferences applicable to drafting views. |
SelectDraftingView Class |
Represents a single object selection. |
SelectDraftingViewList Class |
Represents a list of objects on a selection list. |
SelectDrawingRegion Class |
Represents a single object selection. |
SelectDrawingView Class |
Represents a single object selection. |
SelectDrawingViewList Class |
Represents a list of objects on a selection list. |
SelectModelViewBuilder Class |
Represents a Select Model View builder that selects a model view |
SelectRegionBuilder Class |
Creates the builder for associating the objects from the screen |
SelectSectionLine Class |
Represents a single object selection. |
SettingsBuilder Class |
Represents a Drawings.SettingsBuilder . |
ShadingViewStyle Class |
Represents set of Shading View style applicable to drafting views. |
SheetBorderSettingsBuilder Class |
Represents a NXOpen.Drawings.SheetBorderSettingsBuilder . |
SheetDraftingViewCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.DraftingView`s. |
SheetMarginSettingsBuilder Class |
Represents the Drawing Sheet Margins Style Builder. |
SheetSectionLineCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.SectionLine`s. |
SheetTemplateManager Class |
Represents a manager of :py:class:`NXOpen.Drawings.DraftingView`s. |
SheetZoneReferenceBuilder Class |
builder for creating sheet zone refernce control strings based on the selected attribute and view |
SheetZoneSettingsBuilder Class |
Represents the Drawing Sheet Zone Setting Style Builder. |
ShipDraftingViewLinesBuilder Class |
Represents a ship view lines block |
ShipDraftingViewLinesBuilderList Class |
Represents a list of objects. |
ShipDraftingViewLinesViewStyle Class |
Represents set of Ship Drafting Lines View Style applicable to drafting views. |
ShipbuildingLinesViewStyle Class |
Represents set of Shipbuilding Lines View Style applicable to drafting views. |
SketchSectionLineBuilder Class |
Represents a Drawings.SectionLine builder |
SketchedHalfSectionLine Class |
Sketched Half Section Line is sketch based section line. |
SketchedPointToPointSectionLine Class |
Sketched Point to Point Section Line is sketch based section line. |
SketchedSteppedSectionLine Class |
A Sketched Simple or Stepped Section Line is sketch based section line. |
SmoothEdgesViewStyle Class |
Represents set of Smooth Edges View Style Preferences applicable to drafting views. |
SpecifySectionLineBuilder Class |
Select a section line |
StandardViewsBuilder Class |
This builder allows the user to create a Drawing View |
SteppedSectionLine Class |
A Simple or Stepped Section Line. |
SteppedSectionLineBuilder Class |
Represents a NXOpen.Drawings.SteppedSectionLineBuilder . |
SvtBuilder Class |
Represents a NXOpen.Drawings.SvtBuilder |
ThreadsViewStyle Class |
Represents set of Threads View Style Preferences applicable to drafting views. |
TraceLinesViewStyle Class |
Represents interface for Trace Lines View Style Preferences applicable to drafting views. |
TrackDrawingChangesGeneralBuilder Class |
Represents a NXOpen.Drawings.TrackDrawingChangesGeneralBuilder |
TrackDrawingChangesReportFilterBuilder Class |
Represents a Drawings.TrackDrawingChangesReportFilterBuilder |
UpdateViewsBuilder Class |
Represents a NXOpen.Drawings.UpdateViewsBuilder |
View2dOrientBuilder Class |
Represents the View 2D Orientation (Drawings. |
ViewAlignment Class |
View Alignment object. |
ViewAlignmentBuilder Class |
Represents a NXOpen.Drawings.ViewAlignmentBuilder . |
ViewAlignmentCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.ViewAlignment`s. |
ViewBoundaryBuilder Class |
Represents the View Boundary (Drawings. |
ViewBreak Class |
ViewBreak - defines the portion of a view that gets hidden to produce a broken view |
ViewBreakBuilder Class |
Represents a NXOpen.Drawings.ViewBreakBuilder |
ViewBreakCollection Class |
Represents a collection of :py:class:`NXOpen.Drawings.ViewBreak`s. |
ViewCenterCoordinateBuilder Class |
Represents the View center coodinate (Drawings. |
ViewCommonViewLabelBuilder Class |
Represents a NXOpen.Drawings.ViewCommonViewLabelBuilder |
ViewCopyTo3dBuilder Class |
Represents a NXOpen.Drawings.ViewCopyTo3dBuilder . |
ViewCreationWizardBuilder Class |
This builder allows the user to create a Drawing View |
ViewDetailLabelBuilder Class |
Represents a NXOpen.Drawings.ViewDetailLabelBuilder |
ViewLabelBuilder Class |
Represents a NXOpen.Drawings.ViewLabelBuilder |
ViewOrientationBuilder Class |
Represents a ViewOrientationBuilder. |
ViewPlacementBuilder Class |
Represents a NXOpen.Drawings.ViewPlacementBuilder . |
ViewProjectedArrowSettingsBuilder Class |
Represents a NXOpen.Drawings.ViewProjectedArrowSettingsBuilder |
ViewProjectedLabelBuilder Class |
Represents a NXOpen.Drawings.ViewProjectedLabelBuilder |
ViewProjectedViewSettingsBuilder Class |
Represents a NXOpen.Drawings.ViewProjectedViewSettingsBuilder |
ViewProjectionBuilder Class |
Represents a NXOpen.Drawings.ViewProjectionBuilder . |
ViewProjectionPlaneBuilder Class |
Represents the View Projection Plane (Drawings. |
ViewScaleBuilder Class |
Represents the View Scale (Drawings. |
ViewSectionLabelBuilder Class |
Represents a NXOpen.Drawings.ViewSectionLabelBuilder |
ViewSectionLineBuilder Class |
Represents a NXOpen.Drawings.ViewSectionLineBuilder |
ViewSettingsBuilder Class |
Represents a Drawings.ViewSettingsBuilder . |
ViewStyle Class |
Represents set of style applicable to drafting views. |
ViewStyleBaseBuilder Class |
Represents the BASE tab on the View Style Dialog (Drawings. |
ViewStyleBuilder Class |
Represents the View Style Builder (Drawings. |
ViewStyleDetailBuilder Class |
Represents the DETAIL tab on the View Style Dialog (Drawings. |
ViewStyleFPCalloutConfigBuilder Class |
Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings. |
ViewStyleFPCalloutsBuilder Class |
Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings. |
ViewStyleFPCurvesBuilder Class |
Represents the Curve section of the Flat Pattern tab on the View Style Dialog (Drawings. |
ViewStyleGeneralBuilder Class |
Represents view style general builder (Drawings. |
ViewStyleHiddenLinesBuilder Class |
Represents the HIDDEN LINES tab on the View Style Dialog (Drawings. |
ViewStyleInheritPmiBuilder Class |
Represents the INHERIT PMI tab on the View Style Dialog (Drawings. |
ViewStyleOrientationBuilder Class |
Represents the ORIENTATION tab on the View Style Dialog (Drawings. |
ViewStylePerspectiveBuilder Class |
Represents the PERSPECTIVE tab on the View Style Dialog (Drawings. |
ViewStyleProjectedBuilder Class |
Represents the PROJECTED tab on the View Style Dialog (Drawings. |
ViewStyleSecondaryComponentsBuilder Class |
Represents the Secondary Geometry tab on the View Style Dialog (Drawings. |
ViewStyleSectionBuilder Class |
Represents the SECTION tab on the View Style Dialog (Drawings. |
ViewStyleSectionConstraintsBuilder Class |
Represents the SECTION CONSTRAINTS tab on the View Style Dialog (Drawings. |
ViewStyleShadingBuilder Class |
Represents the SHADING tab on the View Style Dialog (Drawings. |
ViewStyleShipbuildingLinesBuilder Class |
Represents the Shipbuilding LINES tab on the View Style Dialog (Drawings. |
ViewStyleShipbuildingLinesBuilderList Class |
Represents a list of objects. |
ViewStyleSmoothEdgesBuilder Class |
Represents the SMOOTH EDGES tab on the View Style Dialog (Drawings. |
ViewStyleThreadsBuilder Class |
Represents the THREADS tab on the View Style Dialog (Drawings. |
ViewStyleTraceLinesBuilder Class |
Represents the TRACE LINES tab on the View Style Dialog (Drawings. |
ViewStyleVirtualIntersectionsBuilder Class |
Represents the VIRTUAL INTERSECTIONS tab on the View Style Dialog (Drawings. |
ViewStyleVisibleLinesBuilder Class |
Represents the VISIBLE LINES tab on the View Style Dialog (Drawings. |
ViewWorkflowBuilder Class |
Represents a NXOpen.Drawings.ViewWorkflowBuilder |
ViewingDirectionArrow Class |
This class represents a Drafting Viewing Direction Arrow. |
ViewingDirectionArrowLabel Class |
This class represents a Drafting Viewing Direction Arrow Label. |
VirtualIntersectionsViewStyle Class |
Represents set of Virtual Intersections View Style Preferences applicable to drafting views. |
VisibleAndHiddenLinesColorFontWidthBuilder Class |
Represent a NXOpen.Drawings.VisibleAndHiddenLinesColorFontWidthBuilder |
VisibleLinesViewStyle Class |
Represents set of Visible Lines View Style Preferences applicable to drafting views. |
VisualDrawingComparePrefsBuilder Class |
This class gets and sets components of Visual Overlay in Drafting Preferences. |