ViewPlacementBuilderMethod Enumeration

NXOpen.Drawings.ViewPlacementBuilder.Method is an alias for NXOpen.Drawings.ViewPlacementBuilderMethod

class NXOpen.Drawings.ViewPlacementBuilderMethod

Bases: object

view method

Enum Members

Enum Member Enum Member Description
Infer
Infer the view position
Horizontal
Align the view horizontally to another view
Vertical
Align the view vertically to another view
PerpendicularToLine
Align the view along some line to another view
Overlay
Align the view on top of another view
PerpendicularToHingeLine
Align the view along the hinge line
Max
Should be the last enum in the list
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.