TrimmingMarkStyleType Enumeration

class NXOpen.Drawings.TrimmingMarkStyleType

Bases: object

the trimming mark style type Enum Members

Enum Member Enum Member Description
Triangle
Triangle
Corner
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.