ViewScaleBuilderType Enumeration

NXOpen.Drawings.ViewScaleBuilder.Type is an alias for NXOpen.Drawings.ViewScaleBuilderType

class NXOpen.Drawings.ViewScaleBuilderType

Bases: object

The view scale type

Enum Members

Enum Member Enum Member Description
Ratio
determine scale from numerator / denominator
Expression
determine scale from expression
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.