RevolvedSectionLineBuilder Class¶
-
class
NXOpen.Drawings.
RevolvedSectionLineBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.RevolvedSectionLineBuilder
.This class is used to create or edit a
NXOpen.Drawings.RevolvedSectionLine
. .. versionadded:: NX6.0.0Deprecated since version NX10.0.0: Use
Drawings.SectionViewBuilder.SectionViewType()
instead.
Properties¶
Property | Description |
---|---|
EndLocation1 | Returns or sets the end location 1 which determines the position of the first arrow segment in the section line. |
EndLocation2 | Returns or sets the end location 2 which determines the position of the second arrow segment in the section line |
Leg1 | Returns the list of cut and bend segments for the first leg. |
Leg2 | Returns the list of cut and bend segments for the second leg. |
RotationPoint | Returns or sets the rotation point. |
SingleLeg | Returns or sets the single leg indicator. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndLocation1¶
-
RevolvedSectionLineBuilder.
EndLocation1
¶ Returns or sets the end location 1 which determines the position of the first arrow segment in the section line.
-------------------------------------
Getter Method
Signature
EndLocation1()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndLocation1(endLocation1)
Parameters: endLocation1 ( NXOpen.Point
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: drafting (“DRAFTING”)
EndLocation2¶
-
RevolvedSectionLineBuilder.
EndLocation2
¶ Returns or sets the end location 2 which determines the position of the second arrow segment in the section line
-------------------------------------
Getter Method
Signature
EndLocation2()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndLocation2(endLocation2)
Parameters: endLocation2 ( NXOpen.Point
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: drafting (“DRAFTING”)
Leg1¶
-
RevolvedSectionLineBuilder.
Leg1
¶ Returns the list of cut and bend segments for the first leg.
The list will contain
NXOpen.Drawings.SectionLineSegmentBuilderTypes.Cut
andNXOpen.Drawings.SectionLineSegmentBuilderTypes.Bend
types ofNXOpen.Drawings.SectionLineSegmentBuilder
segments.Note that there is no order to the elements of this list since the order is determined by the hinge and arrow direction.
-------------------------------------
Getter Method
Signature
Leg1()
Returns: Return type: NXOpen.Drawings.SectionLineSegmentBuilderList
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
Leg2¶
-
RevolvedSectionLineBuilder.
Leg2
¶ Returns the list of cut and bend segments for the second leg.
This leg is not valid if the single leg indicator is set.
The list will contain
NXOpen.Drawings.SectionLineSegmentBuilderTypes.Cut
andNXOpen.Drawings.SectionLineSegmentBuilderTypes.Bend
types ofNXOpen.Drawings.SectionLineSegmentBuilder
segments.Note that there is no order to the elements of this list since the order is determined by the hinge and arrow direction.
-------------------------------------
Getter Method
Signature
Leg2()
Returns: Return type: NXOpen.Drawings.SectionLineSegmentBuilderList
New in version NX6.0.0.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
License requirements: None.
RotationPoint¶
-
RevolvedSectionLineBuilder.
RotationPoint
¶ Returns or sets the rotation point.
The rotation point identifies position of the axis that the section line is to revolve about.
-------------------------------------
Getter Method
Signature
RotationPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionLineSegmentsBuilder.RotationPoint()
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationPoint(rotationPoint)
Parameters: rotationPoint ( NXOpen.Point
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionLineSegmentsBuilder.RotationPoint()
License requirements: drafting (“DRAFTING”)
SingleLeg¶
-
RevolvedSectionLineBuilder.
SingleLeg
¶ Returns or sets the single leg indicator.
Set this flag to true to create a revolved section line that contains only one leg.
-------------------------------------
Getter Method
Signature
SingleLeg()
Returns: Return type: bool New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionLineSegmentsBuilder.SingleLeg()
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleLeg(singleLeg)
Parameters: singleLeg (bool) – New in version NX6.0.0.
Deprecated since version NX10.0.0: Use
Drawings.SectionLineSegmentsBuilder.SingleLeg()
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
RevolvedSectionLineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.