Properties¶
Property | Description |
---|---|
Color | Returns or sets the color on the HIDDEN LINES tab of the View Style Dialog |
EdgesHiddenByEdges | Returns or sets the edges hidden by edges toggle on the HIDDEN LINES tab of the View Style Dialog |
Font | Returns or sets the font on the HIDDEN LINES tab of the View Style Dialog |
HiddenLine | Returns or sets the hidden line toggle on the HIDDEN LINES tab of the View Style Dialog |
IncludeModelCurves | Returns or sets the include model curves toggle on the HIDDEN LINES tab of the View Style Dialog |
InterferingSolids | Returns or sets the interfering solids toggle on the HIDDEN LINES tab of the View Style Dialog |
ReferenceEdgesOnly | Returns or sets the reference edges only toggle on the HIDDEN LINES tab of the View Style Dialog |
SelfHidden | Returns or sets the self hidden toggle on the HIDDEN LINES tab of the View Style Dialog |
SmallFeature | Returns or sets the small feature option on the HIDDEN LINES tab of the View Style Dialog |
SmallFeaturesTolerance | Returns or sets the small features tolerance on the HIDDEN LINES tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Width | Returns or sets the width on the HIDDEN LINES tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Color¶
-
ViewStyleHiddenLinesBuilder.
Color
¶ Returns or sets the color on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Color()
Returns: Returns the color that is on the hidden line sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – Sets a new color on the hidden line sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Font¶
-
ViewStyleHiddenLinesBuilder.
Font
¶ Returns or sets the font on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Font()
Returns: Returns the font that is on the hidden line sub-builder Return type: NXOpen.Preferences.Font
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Font(font)
Parameters: font ( NXOpen.Preferences.Font
) – Sets a new font on the hidden line sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
IncludeModelCurves¶
-
ViewStyleHiddenLinesBuilder.
IncludeModelCurves
¶ Returns or sets the include model curves toggle on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
IncludeModelCurves()
Returns: Returns the include model curves toggle value that is on the hidden line sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeModelCurves(includeModelCurvesToggle)
Parameters: includeModelCurvesToggle (bool) – Sets a new include model curves toggle value on the hidden line sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
InterferingSolids¶
-
ViewStyleHiddenLinesBuilder.
InterferingSolids
¶ Returns or sets the interfering solids toggle on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
InterferingSolids()
Returns: Returns the interfering solids toggle value that is on the hidden line sub-builder Return type: NXOpen.Preferences.HiddenLineInterferingSolidsOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterferingSolids(interferingSolidsOption)
Parameters: interferingSolidsOption ( NXOpen.Preferences.HiddenLineInterferingSolidsOption
) – Sets a new interfering solids toggle value on the hidden line sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ReferenceEdgesOnly¶
-
ViewStyleHiddenLinesBuilder.
ReferenceEdgesOnly
¶ Returns or sets the reference edges only toggle on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ReferenceEdgesOnly()
Returns: Returns the reference edges only toggle value that is on the hidden line sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceEdgesOnly(referenceEdgesOnlyToggle)
Parameters: referenceEdgesOnlyToggle (bool) – Sets a new reference edges only toggle value on the hidden line sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SmallFeature¶
-
ViewStyleHiddenLinesBuilder.
SmallFeature
¶ Returns or sets the small feature option on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
SmallFeature()
Returns: Returns the small feature option that is on the hidden line sub-builder Return type: NXOpen.Preferences.HiddenLineSmallFeatureOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmallFeature(smallFeatureOption)
Parameters: smallFeatureOption ( NXOpen.Preferences.HiddenLineSmallFeatureOption
) – Sets a new small feature option on the hidden line sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SmallFeaturesTolerance¶
-
ViewStyleHiddenLinesBuilder.
SmallFeaturesTolerance
¶ Returns or sets the small features tolerance on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
SmallFeaturesTolerance()
Returns: Returns the small features tolerance value that is on the hidden line sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmallFeaturesTolerance(smallFeaturesTolerance)
Parameters: smallFeaturesTolerance (float) – Sets a new small features tolerance value on the hidden line sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Width¶
-
ViewStyleHiddenLinesBuilder.
Width
¶ Returns or sets the width on the HIDDEN LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Width()
Returns: Returns the width that is on the hidden line sub-builder Return type: NXOpen.Preferences.Width
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.Preferences.Width
) – Sets a new width on the hidden line sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleHiddenLinesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.