HiddenLineSmallFeatureOption Enumeration

class NXOpen.Preferences.HiddenLineSmallFeatureOption

Bases: object

Represents the small feature options Enum Members

Enum Member Enum Member Description
ShowAll
Show All
Simplify
Simplify
Hide
Hide
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.