SectionLineSegmentPointListBuilder Class¶
-
class
NXOpen.Drawings.
SectionLineSegmentPointListBuilder
¶ Bases:
NXOpen.TaggedObject
Represents SectionLineSegmentPointListBuilder class.
This class maintains a list of
NXOpen.Drawings.SectionLineSegmentPointBuilder
objects and manages them.New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Length | Returns the number of NXOpen.Drawings.SectionLineSegmentPointBuilder objects in the list |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Length¶
-
SectionLineSegmentPointListBuilder.
Length
¶ Returns the number of
NXOpen.Drawings.SectionLineSegmentPointBuilder
objects in the list-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: int New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
AddCutSegment¶
-
SectionLineSegmentPointListBuilder.
AddCutSegment
¶ Overloaded method AddCutSegment
AddCutSegment(location)
AddCutSegment(location, referencedCutSegment)
-------------------------------------
Creates a new
NXOpen.Drawings.SectionLineSegmentPointBuilder
objectSignature
AddCutSegment(location)
Parameters: location ( NXOpen.Point
) –Returns: Return type: NXOpen.Drawings.SectionLineSegmentPointBuilder
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Creates a new
NXOpen.Drawings.SectionLineSegmentPointBuilder
In case of point to point section line ,new segment is added at location prior to reference cut segment specified. If reference cut segment is not specified , new segment is added prior to last arrow segment.Signature
AddCutSegment(location, referencedCutSegment)
Parameters: - location (
NXOpen.Point
) – - referencedCutSegment (
NXOpen.Drawings.SectionLineSegmentPointBuilder
) – reference SectionLineSegmentPointBuilder
Returns: Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
Append¶
-
SectionLineSegmentPointListBuilder.
Append
¶ Appends
NXOpen.Drawings.SectionLineSegmentPointBuilder
object to the end of the listSignature
Append(pointData)
Parameters: pointData ( NXOpen.Drawings.SectionLineSegmentPointBuilder
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Clear¶
-
SectionLineSegmentPointListBuilder.
Clear
¶ Deletes all
NXOpen.Drawings.SectionLineSegmentPointBuilder
objects from the listSignature
Clear()
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
CreateSectionLineSegmentPointBuilder¶
-
SectionLineSegmentPointListBuilder.
CreateSectionLineSegmentPointBuilder
¶ Creates a new
NXOpen.Drawings.SectionLineSegmentPointBuilder
objectSignature
CreateSectionLineSegmentPointBuilder()
Returns: Return type: NXOpen.Drawings.SectionLineSegmentPointBuilder
New in version NX10.0.0.
License requirements: None.
Delete¶
-
SectionLineSegmentPointListBuilder.
Delete
¶ Overloaded method Delete
Delete(point)
Delete(index)
-------------------------------------
Deletes a given
NXOpen.Drawings.SectionLineSegmentPointBuilder
object from the listSignature
Delete(point)
Parameters: point ( NXOpen.Drawings.SectionLineSegmentPointBuilder
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Deletes
NXOpen.Drawings.SectionLineSegmentPointBuilder
object of a certain index from the listSignature
Delete(index)
Parameters: index (int) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
FindItem¶
-
SectionLineSegmentPointListBuilder.
FindItem
¶ Returns
NXOpen.Drawings.SectionLineSegmentPointBuilder
object at the input index.May be NULL if not found.
Signature
FindItem(index)
Parameters: index (int) – index of object to return Returns: object found at input index Return type: NXOpen.Drawings.SectionLineSegmentPointBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
GetContents¶
-
SectionLineSegmentPointListBuilder.
GetContents
¶ Queries all the
NXOpen.Drawings.SectionLineSegmentPointBuilder
objectsSignature
GetContents()
Returns: Return type: list of NXOpen.Drawings.SectionLineSegmentPointBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
GetIndex¶
-
SectionLineSegmentPointListBuilder.
GetIndex
¶ Finds index of
NXOpen.Drawings.SectionLineSegmentPointBuilder
object in the listSignature
GetIndex(point)
Parameters: point ( NXOpen.Drawings.SectionLineSegmentPointBuilder
) –Returns: Equals -1 if not found Return type: int New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Insert¶
-
SectionLineSegmentPointListBuilder.
Insert
¶ Inserts
NXOpen.Drawings.SectionLineSegmentPointBuilder
object in the list before a given positionSignature
Insert(insertBeforeIndex, point)
Parameters: - insertBeforeIndex (int) –
- point (
NXOpen.Drawings.SectionLineSegmentPointBuilder
) –
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
MoveSegment¶
-
SectionLineSegmentPointListBuilder.
MoveSegment
¶ Moves a given
NXOpen.Drawings.SectionLineSegmentPointBuilder
object from the listSignature
MoveSegment(point, pointspecified)
Parameters: - point (
NXOpen.Drawings.SectionLineSegmentPointBuilder
) – - pointspecified (
NXOpen.Point
) –
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
- point (
SetContents¶
-
SectionLineSegmentPointListBuilder.
SetContents
¶ Sets array of
NXOpen.Drawings.SectionLineSegmentPointBuilder
objects in the list.Signature
SetContents(points)
Parameters: points (list of NXOpen.Drawings.SectionLineSegmentPointBuilder
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)