SectionLineSegmentPointBuilder Class¶
-
class
NXOpen.Drawings.
SectionLineSegmentPointBuilder
¶ Bases:
NXOpen.TaggedObject
Represents Section Line Segment Point Builder
To create a new instance of this class, use
NXOpen.Drawings.SectionLineSegmentPointListBuilder.CreateSectionLineSegmentPointBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Point | Returns or sets the section line segment NXOpen.Point |
SegmentType | Returns or sets the segment type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
SectionLineSegmentPointBuilderSegmentTypes Enumeration | Section Segment Types |
Property Detail¶
Point¶
-
SectionLineSegmentPointBuilder.
Point
¶ Returns or sets the section line segment
NXOpen.Point
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
SegmentType¶
-
SectionLineSegmentPointBuilder.
SegmentType
¶ Returns or sets the segment type
-------------------------------------
Getter Method
Signature
SegmentType()
Returns: Return type: NXOpen.Drawings.SectionLineSegmentPointBuilderSegmentTypes
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
SegmentType(type)
Parameters: type ( NXOpen.Drawings.SectionLineSegmentPointBuilderSegmentTypes
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)