BordersAndZonesCollection Class

class NXOpen.Drawings.BordersAndZonesCollection

Bases: object

Represents a collection of NXOpen.Drawings.BordersAndZones objects

To obtain an instance of this class, refer to NXOpen.DraftingManager

New in version NX8.0.0.

Methods

Method Description
CreateBordersAndZonesBuilder Creates a borders and zones builder @return BordersAndZonesBuilder object
FindObject Finds the NXOpen.Drawings.BordersAndZones with the given name.

Method Detail

CreateBordersAndZonesBuilder

BordersAndZonesCollection.CreateBordersAndZonesBuilder

Creates a borders and zones builder

Signature CreateBordersAndZonesBuilder(bordersAndZones)

Parameters:bordersAndZones (NXOpen.Drawings.BordersAndZones) – NXOpen.Drawings.BordersAndZones to be redefined, if None then creates a new one
Returns:BordersAndZonesBuilder object
Return type:NXOpen.Drawings.BordersAndZonesBuilder

New in version NX8.0.0.

License requirements: drafting (“DRAFTING”)

FindObject

BordersAndZonesCollection.FindObject

Finds the NXOpen.Drawings.BordersAndZones with the given name.

An exception will be thrown if no object can be found with the given name.

Signature FindObject(name)

Parameters:name (str) – Drawing sheet name
Returns:Borders and zones object
Return type:NXOpen.Drawings.BordersAndZones

New in version NX8.0.0.

License requirements: None.