BrokenViewBuilderTypeDirection Enumeration

NXOpen.Drawings.BrokenViewBuilder.TypeDirection is an alias for NXOpen.Drawings.BrokenViewBuilderTypeDirection

class NXOpen.Drawings.BrokenViewBuilderTypeDirection

Bases: object

Direction Enum

Enum Members

Enum Member Enum Member Description
Parallel
Parallel
Perpendicular
Perpendicular
Vector
Specified by Vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.