ViewStyleProjectedBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleProjectedBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the PROJECTED tab on the View Style Dialog (Drawings.
ViewStyleProjectedBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Align | Returns or sets the projected view style align toggle on the PROJECTED tab of the View Style Dialog |
Gdt | Returns or sets the projected view style gdt toggle on the PROJECTED tab of the View Style Dialog |
Offset | Returns or sets the projected view style offset toggle on the PROJECTED tab of the View Style Dialog |
Orient | Returns or sets the projected view style orient toggle on the PROJECTED tab of the View Style Dialog |
Scale | Returns or sets the projected view style scale toggle on the PROJECTED tab of the View Style Dialog |
Sheet | Returns or sets the projected view style sheet toggle on the PROJECTED tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Align¶
-
ViewStyleProjectedBuilder.
Align
¶ Returns or sets the projected view style align toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Align()
Returns: Returns the align toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Align(alignToggle)
Parameters: alignToggle (bool) – Sets a new align toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Gdt¶
-
ViewStyleProjectedBuilder.
Gdt
¶ Returns or sets the projected view style gdt toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Gdt()
Returns: Returns the gdt toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Gdt(gdtToggle)
Parameters: gdtToggle (bool) – Sets a new gdt toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Offset¶
-
ViewStyleProjectedBuilder.
Offset
¶ Returns or sets the projected view style offset toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Offset()
Returns: Returns the offset toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offsetToggle)
Parameters: offsetToggle (bool) – Sets a new offset toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Orient¶
-
ViewStyleProjectedBuilder.
Orient
¶ Returns or sets the projected view style orient toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Orient()
Returns: Returns the orient toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Orient(orientToggle)
Parameters: orientToggle (bool) – Sets a new orient toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Scale¶
-
ViewStyleProjectedBuilder.
Scale
¶ Returns or sets the projected view style scale toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Scale()
Returns: Returns the scale toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scaleToggle)
Parameters: scaleToggle (bool) – Sets a new scale toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Sheet¶
-
ViewStyleProjectedBuilder.
Sheet
¶ Returns or sets the projected view style sheet toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Sheet()
Returns: Returns the sheet toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sheet(sheetToggle)
Parameters: sheetToggle (bool) – Sets a new sheet toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleProjectedBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.