ViewProjectionBuilderTypes Enumeration

NXOpen.Drawings.ViewProjectionBuilder.Types is an alias for NXOpen.Drawings.ViewProjectionBuilderTypes

class NXOpen.Drawings.ViewProjectionBuilderTypes

Bases: object

the type of view projection

Enum Members

Enum Member Enum Member Description
ProjectOnOnePlane
on one plane
ProjectOnTwoPlanes
on two planes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.