ViewSectionLabelBuilder Class

class NXOpen.Drawings.ViewSectionLabelBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Drawings.ViewSectionLabelBuilder

New in version NX9.0.0.

Properties

Property Description
CustomizedViewLabel Returns or sets the customized view label
IncludeParentheses Returns or sets the include parentheses
IncludeRotationAngle Returns or sets the include rotation angle
IncludeRotationSymbol Returns or sets the include rotation symbol
LabelCharacterHeightFactor Returns or sets the label character height factor
LabelPosition Returns or sets the label position
LabelPrefix Returns or sets the label prefix
LetterFormat Returns or sets the letter format
PrefixCharacterHeightFactor Returns or sets the prefix character height factor
ReferenceToShow Returns or sets the reference to show
ScaleCharacterHeightFactor Returns or sets the scale character height factor
ScalePosition Returns or sets the scale position
ScalePrefix Returns or sets the scale prefix
ShowViewLabel Returns or sets the show view label
ShowViewScale Returns or sets the show view scale
Tag Returns the Tag for this object.
ValueFormat Returns or sets the section vw label scale value format
ViewLabelOption Returns or sets the view label option

Methods

Method Description
GetCustomizedViewLabelText Returns the customized view label text @return
SetCustomizedViewLabelText Sets the customized view label text
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CustomizedViewLabel

ViewSectionLabelBuilder.CustomizedViewLabel

Returns or sets the customized view label

-------------------------------------

Getter Method

Signature CustomizedViewLabel()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CustomizedViewLabel(customizedViewLabel)

Parameters:customizedViewLabel (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

IncludeParentheses

ViewSectionLabelBuilder.IncludeParentheses

Returns or sets the include parentheses

-------------------------------------

Getter Method

Signature IncludeParentheses()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IncludeParentheses(includeParentheses)

Parameters:includeParentheses (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

IncludeRotationAngle

ViewSectionLabelBuilder.IncludeRotationAngle

Returns or sets the include rotation angle

-------------------------------------

Getter Method

Signature IncludeRotationAngle()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IncludeRotationAngle(includeRotationAngle)

Parameters:includeRotationAngle (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

IncludeRotationSymbol

ViewSectionLabelBuilder.IncludeRotationSymbol

Returns or sets the include rotation symbol

-------------------------------------

Getter Method

Signature IncludeRotationSymbol()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IncludeRotationSymbol(includeRotationSymbol)

Parameters:includeRotationSymbol (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

LabelCharacterHeightFactor

ViewSectionLabelBuilder.LabelCharacterHeightFactor

Returns or sets the label character height factor

-------------------------------------

Getter Method

Signature LabelCharacterHeightFactor()

Returns:
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelCharacterHeightFactor(labelCharacterHeightFactor)

Parameters:labelCharacterHeightFactor (float) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

LabelPosition

ViewSectionLabelBuilder.LabelPosition

Returns or sets the label position

-------------------------------------

Getter Method

Signature LabelPosition()

Returns:
Return type:NXOpen.Drawings.LabelPositionTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelPosition(labelPosition)

Parameters:labelPosition (NXOpen.Drawings.LabelPositionTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

LabelPrefix

ViewSectionLabelBuilder.LabelPrefix

Returns or sets the label prefix

-------------------------------------

Getter Method

Signature LabelPrefix()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelPrefix(labelPrefix)

Parameters:labelPrefix (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

LetterFormat

ViewSectionLabelBuilder.LetterFormat

Returns or sets the letter format

-------------------------------------

Getter Method

Signature LetterFormat()

Returns:
Return type:NXOpen.Drawings.LetterFormatTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LetterFormat(letterFormat)

Parameters:letterFormat (NXOpen.Drawings.LetterFormatTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

PrefixCharacterHeightFactor

ViewSectionLabelBuilder.PrefixCharacterHeightFactor

Returns or sets the prefix character height factor

-------------------------------------

Getter Method

Signature PrefixCharacterHeightFactor()

Returns:
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PrefixCharacterHeightFactor(prefixCharacterHeightFactor)

Parameters:prefixCharacterHeightFactor (float) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ReferenceToShow

ViewSectionLabelBuilder.ReferenceToShow

Returns or sets the reference to show

-------------------------------------

Getter Method

Signature ReferenceToShow()

Returns:
Return type:NXOpen.Drawings.ReferenceShowTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReferenceToShow(referenceToShow)

Parameters:referenceToShow (NXOpen.Drawings.ReferenceShowTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ScaleCharacterHeightFactor

ViewSectionLabelBuilder.ScaleCharacterHeightFactor

Returns or sets the scale character height factor

-------------------------------------

Getter Method

Signature ScaleCharacterHeightFactor()

Returns:
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScaleCharacterHeightFactor(scaleCharacterHeightFactor)

Parameters:scaleCharacterHeightFactor (float) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ScalePosition

ViewSectionLabelBuilder.ScalePosition

Returns or sets the scale position

-------------------------------------

Getter Method

Signature ScalePosition()

Returns:
Return type:NXOpen.Drawings.ScalePositionTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScalePosition(scalePosition)

Parameters:scalePosition (NXOpen.Drawings.ScalePositionTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ScalePrefix

ViewSectionLabelBuilder.ScalePrefix

Returns or sets the scale prefix

-------------------------------------

Getter Method

Signature ScalePrefix()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScalePrefix(scalePrefix)

Parameters:scalePrefix (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ShowViewLabel

ViewSectionLabelBuilder.ShowViewLabel

Returns or sets the show view label

-------------------------------------

Getter Method

Signature ShowViewLabel()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowViewLabel(showViewLabel)

Parameters:showViewLabel (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ShowViewScale

ViewSectionLabelBuilder.ShowViewScale

Returns or sets the show view scale

-------------------------------------

Getter Method

Signature ShowViewScale()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowViewScale(showViewScale)

Parameters:showViewScale (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ValueFormat

ViewSectionLabelBuilder.ValueFormat

Returns or sets the section vw label scale value format

-------------------------------------

Getter Method

Signature ValueFormat()

Returns:
Return type:NXOpen.Drawings.ScaleValueFormatTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ValueFormat(valueFormat)

Parameters:valueFormat (NXOpen.Drawings.ScaleValueFormatTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ViewLabelOption

ViewSectionLabelBuilder.ViewLabelOption

Returns or sets the view label option

-------------------------------------

Getter Method

Signature ViewLabelOption()

Returns:
Return type:NXOpen.Drawings.ViewLabelTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ViewLabelOption(viewLabelOption)

Parameters:viewLabelOption (NXOpen.Drawings.ViewLabelTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

GetCustomizedViewLabelText

ViewSectionLabelBuilder.GetCustomizedViewLabelText

Returns the customized view label text

Signature GetCustomizedViewLabelText()

Returns:
Return type:list of str

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

SetCustomizedViewLabelText

ViewSectionLabelBuilder.SetCustomizedViewLabelText

Sets the customized view label text

Signature SetCustomizedViewLabelText(customizedText)

Parameters:customizedText (list of str) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

Validate

ViewSectionLabelBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.