BrokenViewBuilderLineWidth Enumeration

NXOpen.Drawings.BrokenViewBuilder.LineWidth is an alias for NXOpen.Drawings.BrokenViewBuilderLineWidth

class NXOpen.Drawings.BrokenViewBuilderLineWidth

Bases: object

Line Width

Enum Members

Enum Member Enum Member Description
Thin
Thin
Medium
Medium
Thick
Thick
WidthOne
Width One
WidthTwo
Width Two
WidthThree
Width Three
WidthFour
Width Four
WidthFive
Width Five
WidthSix
Width Six
WidthSeven
Width Seven
WidthEight
Width Eight
WidthNine
Width Nine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.