DetailViewBuilderTypes Enumeration¶
NXOpen.Drawings.DetailViewBuilder.Types is an alias for NXOpen.Drawings.DetailViewBuilderTypes
-
class
NXOpen.Drawings.
DetailViewBuilderTypes
¶ Bases:
object
the type of boundary
Enum Members
Enum Member Enum Member Description Undefined For initial valuesCircular Circular boundaryRectangleByCorners Rectangular boundary defined by two cornersRectangleByCenterAndCorner Rectangular boundary defined by the center and a cornerCustom Custom boundary (this should not be used unless the detail view already has a custom boundary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-