DrawingSheetBuilderSheetUnits Enumeration

NXOpen.Drawings.DrawingSheetBuilder.SheetUnits is an alias for NXOpen.Drawings.DrawingSheetBuilderSheetUnits

class NXOpen.Drawings.DrawingSheetBuilderSheetUnits

Bases: object

the drawing sheet units

Enum Members

Enum Member Enum Member Description
Metric
a Metric units drawing sheet
English
an English units drawing sheet
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.