ConvertDraftingContentsBuilder Class¶
-
class
NXOpen.Drawings.
ConvertDraftingContentsBuilder
¶ Bases:
NXOpen.Builder
Represents a
Drawings.ConvertDraftingContentsBuilder
.This class queries and sets settings specific to drafting data which will get converted to PMI.
To create a new instance of this class, use
NXOpen.Drawings.ConvertToPMIBuilderManager.CreateConvertDraftingContentsBuilder()
Default values.
Property Value SelectionType Drawing UseContextAssembly 0 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ConfigurationFile | Returns or sets the configuration file |
SelectDraftingSheet | Returns the select drafting sheet block |
SelectDraftingView | Returns the select drafting view block |
SelectObjectsToConvert | Returns the select objects to convert |
SelectionType | Returns or sets the selection type |
SettingsBuilder | Returns the settings |
Tag | Returns the Tag for this object. |
UseContextAssembly | Returns or sets the use context assembly |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetContextAssembly | Context assembly part file path |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConvertDraftingContentsBuilderSelectConversionEntityType Enumeration | enum is used to list out different entity that can be use for conversion |
Property Detail¶
ConfigurationFile¶
-
ConvertDraftingContentsBuilder.
ConfigurationFile
¶ Returns or sets the configuration file
-------------------------------------
Getter Method
Signature
ConfigurationFile()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfigurationFile(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: convert_to_pmi (” Convert To PMI”), drafting (“DRAFTING”)
SelectDraftingSheet¶
-
ConvertDraftingContentsBuilder.
SelectDraftingSheet
¶ Returns the select drafting sheet block
-------------------------------------
Getter Method
Signature
SelectDraftingSheet()
Returns: Return type: NXOpen.Drawings.SelectDraftingViewList
New in version NX11.0.0.
License requirements: None.
SelectDraftingView¶
-
ConvertDraftingContentsBuilder.
SelectDraftingView
¶ Returns the select drafting view block
-------------------------------------
Getter Method
Signature
SelectDraftingView()
Returns: Return type: NXOpen.Drawings.SelectDraftingViewList
New in version NX11.0.0.
License requirements: None.
SelectObjectsToConvert¶
-
ConvertDraftingContentsBuilder.
SelectObjectsToConvert
¶ Returns the select objects to convert
-------------------------------------
Getter Method
Signature
SelectObjectsToConvert()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
SelectionType¶
-
ConvertDraftingContentsBuilder.
SelectionType
¶ Returns or sets the selection type
-------------------------------------
Getter Method
Signature
SelectionType()
Returns: Return type: NXOpen.Drawings.ConvertDraftingContentsBuilderSelectConversionEntityType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionType(selectionType)
Parameters: selectionType ( NXOpen.Drawings.ConvertDraftingContentsBuilderSelectConversionEntityType
) –New in version NX11.0.0.
License requirements: convert_to_pmi (” Convert To PMI”), drafting (“DRAFTING”)
SettingsBuilder¶
-
ConvertDraftingContentsBuilder.
SettingsBuilder
¶ Returns the settings
-------------------------------------
Getter Method
Signature
SettingsBuilder()
Returns: Return type: NXOpen.Drawings.SettingsBuilder
New in version NX11.0.0.
License requirements: None.
UseContextAssembly¶
-
ConvertDraftingContentsBuilder.
UseContextAssembly
¶ Returns or sets the use context assembly
-------------------------------------
Getter Method
Signature
UseContextAssembly()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseContextAssembly(useContextAssembly)
Parameters: useContextAssembly (bool) – New in version NX11.0.0.
License requirements: convert_to_pmi (” Convert To PMI”), drafting (“DRAFTING”)
Method Detail¶
SetContextAssembly¶
-
ConvertDraftingContentsBuilder.
SetContextAssembly
¶ Context assembly part file path
Signature
SetContextAssembly(contextAssembly)
Parameters: contextAssembly (str) – New in version NX11.0.0.
License requirements: convert_to_pmi (” Convert To PMI”), drafting (“DRAFTING”)
Validate¶
-
ConvertDraftingContentsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.