SettingsBuilder Class¶
-
class
NXOpen.Drawings.
SettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
Drawings.SettingsBuilder
.This class queries and sets settings.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AnnotationSettings | Returns the Annotation settings builder which stores the annotation settings |
ConversionSettings | Returns the Component settings builder which stores the component settings |
Tag | Returns the Tag for this object. |
ViewSettings | Returns the View settings builder which stores the view settings |
Methods¶
Method | Description |
---|---|
SaveConfigurationFile | API used to save settings data |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnnotationSettings¶
-
SettingsBuilder.
AnnotationSettings
¶ Returns the Annotation settings builder which stores the annotation settings
-------------------------------------
Getter Method
Signature
AnnotationSettings()
Returns: Return type: NXOpen.Drawings.AnnotationSettingsBuilder
New in version NX11.0.0.
License requirements: None.
ConversionSettings¶
-
SettingsBuilder.
ConversionSettings
¶ Returns the Component settings builder which stores the component settings
-------------------------------------
Getter Method
Signature
ConversionSettings()
Returns: Return type: NXOpen.Drawings.ConversionProcessSettingsBuilder
New in version NX11.0.0.
License requirements: None.
ViewSettings¶
-
SettingsBuilder.
ViewSettings
¶ Returns the View settings builder which stores the view settings
-------------------------------------
Getter Method
Signature
ViewSettings()
Returns: Return type: NXOpen.Drawings.ViewSettingsBuilder
New in version NX11.0.0.
License requirements: None.
Method Detail¶
SaveConfigurationFile¶
-
SettingsBuilder.
SaveConfigurationFile
¶ API used to save settings data
Signature
SaveConfigurationFile(saveAsFile)
Parameters: saveAsFile (str) – New in version NX11.0.0.
License requirements: convert_to_pmi (” Convert To PMI”), drafting (“DRAFTING”)
Validate¶
-
SettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.