MultipleViewPlacementBuilderOption Enumeration

NXOpen.Drawings.MultipleViewPlacementBuilder.Option is an alias for NXOpen.Drawings.MultipleViewPlacementBuilderOption

class NXOpen.Drawings.MultipleViewPlacementBuilderOption

Bases: object

The placement option type

Enum Members

Enum Member Enum Member Description
Center
By Center
Corners
By Corners
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.