ViewBoundaryBuilder Class¶
-
class
NXOpen.Drawings.
ViewBoundaryBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the View Boundary (Drawings.
ViewBoundaryBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BoundaryPoint1 | Returns or sets the first corner point |
BoundaryPoint2 | Returns or sets the second corner point |
BoundaryType | Returns or sets the orientation type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ViewBoundaryBuilderType Enumeration | The view boundary type |
Property Detail¶
BoundaryPoint1¶
-
ViewBoundaryBuilder.
BoundaryPoint1
¶ Returns or sets the first corner point
-------------------------------------
Getter Method
Signature
BoundaryPoint1()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryPoint1(boundaryPoint1)
Parameters: boundaryPoint1 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_layout (“NX Layout”)
BoundaryPoint2¶
-
ViewBoundaryBuilder.
BoundaryPoint2
¶ Returns or sets the second corner point
-------------------------------------
Getter Method
Signature
BoundaryPoint2()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryPoint2(boundaryPoint2)
Parameters: boundaryPoint2 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_layout (“NX Layout”)
BoundaryType¶
-
ViewBoundaryBuilder.
BoundaryType
¶ Returns or sets the orientation type
-------------------------------------
Getter Method
Signature
BoundaryType()
Returns: returns the boundary type. Return type: NXOpen.Drawings.ViewBoundaryBuilderType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryType(type)
Parameters: type ( NXOpen.Drawings.ViewBoundaryBuilderType
) – sets the boundary type.New in version NX6.0.0.
License requirements: nx_layout (“NX Layout”)
Method Detail¶
Validate¶
-
ViewBoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.