ShipDraftingViewLinesViewStyleLines Enumeration¶
NXOpen.Drawings.ShipDraftingViewLinesViewStyle.Lines is an alias for NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
-
class
NXOpen.Drawings.
ShipDraftingViewLinesViewStyleLines
¶ Bases:
object
Line type
Enum Members
Enum Member Enum Member Description HiddenNonsection Hidden, NonSectionVisibleNonsection Visible, NonSectionHiddenSection Hidden, SectionVisibleSection Visible, SectionSecondaryHiddenNonsection Secondary, Hidden, NonSectionSecondaryVisibleNonsection Secondary, Visible, NonSectionSecondaryHiddenSection Secondary, Hidden, SectionSecondaryVisibleSection Secondary, Visible, Section-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-