DrawingSheetStandardSheetSize Enumeration

NXOpen.Drawings.DrawingSheet.StandardSheetSize is an alias for NXOpen.Drawings.DrawingSheetStandardSheetSize

class NXOpen.Drawings.DrawingSheetStandardSheetSize

Bases: object

Standard Drawing sizes

Enum Members

Enum Member Enum Member Description
A
8.5 x 11 inches
B
11 X 17 inches
C
17 X 22 inches
D
22 X 34 inches
E
34 X 44 inches
F
28 X 40 inches
H
28 X 44 inches
J
34 X 55 inches
A0
841 x 1189 millimeters
A1
594 X 841 millimeters
A2
420 X 594 millimeters
A3
297 X 420 millimeters
A4
210 X 297 millimeters
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.