DetailViewBuilder Class¶
-
class
NXOpen.Drawings.
DetailViewBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Drawings.DetailView
.This class is used to create and edit Detail Views
To create a new instance of this class, use
NXOpen.Drawings.DraftingViewCollection.CreateDetailViewBuilder()
Default values.
Property Value Origin.AlignmentMethod Infer Origin.AlignmentOption ToView Scale.Denominator 1.0 Scale.Numerator 1.0 Scale.ScaleType Ratio SecondaryComponents.ObjectType PrimaryGeometry Style.ViewStyleGeneral.AngleValue 0.0 Style.ViewStyleOrientation.HingeLine.ReverseDirection false Style.ViewStyleOrientation.HingeLine.VectorOption Inferred Style.ViewStyleOrientation.Ovt.AssociativeOrientation 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative toggle If view is associative and set associative to false, the view will be converted to independent detail view. |
BoundaryPoint1 | Returns or sets the first boundary point. |
BoundaryPoint2 | Returns or sets the second boundary point. |
HiddenObjects | Returns the list of objects to not show in the view |
LabelOnParent | Returns or sets the label on parent |
NonSectionedObjects | Returns the list of objects to not section in the view |
Origin | Returns the origin |
Parent | Returns the parent view |
Scale | Returns the scale |
SecondaryComponents | Returns the list of secondary components in the view |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DetailViewBuilderLabelOnParentType Enumeration | the display type for the label on parent |
DetailViewBuilderTypes Enumeration | the type of boundary |
Property Detail¶
Associative¶
-
DetailViewBuilder.
Associative
¶ Returns or sets the associative toggle If view is associative and set associative to false, the view will be converted to independent detail view.
Otherwise, this setting will have no effect
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX7.5.0.
License requirements: None.
BoundaryPoint1¶
-
DetailViewBuilder.
BoundaryPoint1
¶ Returns or sets the first boundary point.
This is the center of the boundary for these types:
NXOpen.Drawings.DetailViewBuilderTypes.Circular
andNXOpen.Drawings.DetailViewBuilderTypes.RectangleByCenterAndCorner
-------------------------------------
Getter Method
Signature
BoundaryPoint1()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryPoint1(boundaryPoint1)
Parameters: boundaryPoint1 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
BoundaryPoint2¶
-
DetailViewBuilder.
BoundaryPoint2
¶ Returns or sets the second boundary point.
This is the point on the circle for the
NXOpen.Drawings.DetailViewBuilderTypes.Circular
and the corner point for theNXOpen.Drawings.DetailViewBuilderTypes.RectangleByCenterAndCorner
.-------------------------------------
Getter Method
Signature
BoundaryPoint2()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryPoint2(boundaryPoint2)
Parameters: boundaryPoint2 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
LabelOnParent¶
-
DetailViewBuilder.
LabelOnParent
¶ Returns or sets the label on parent
-------------------------------------
Getter Method
Signature
LabelOnParent()
Returns: Return type: NXOpen.Drawings.DetailViewBuilderLabelOnParentType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelOnParent(labelOnParent)
Parameters: labelOnParent ( NXOpen.Drawings.DetailViewBuilderLabelOnParentType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
NonSectionedObjects¶
-
DetailViewBuilder.
NonSectionedObjects
¶ Returns the list of objects to not section in the view
-------------------------------------
Getter Method
Signature
NonSectionedObjects()
Returns: Return type: NXOpen.Drawings.HiddenObjectsBuilder
New in version NX6.0.0.
License requirements: None.
Origin¶
-
DetailViewBuilder.
Origin
¶ Returns the origin
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Drawings.ViewPlacementBuilder
New in version NX6.0.0.
License requirements: None.
Parent¶
-
DetailViewBuilder.
Parent
¶ Returns the parent view
-------------------------------------
Getter Method
Signature
Parent()
Returns: Return type: NXOpen.Drawings.ParentViewBuilder
New in version NX6.0.0.
License requirements: None.
Scale¶
-
DetailViewBuilder.
Scale
¶ Returns the scale
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: NXOpen.Drawings.ViewScaleBuilder
New in version NX6.0.0.
License requirements: None.
SecondaryComponents¶
-
DetailViewBuilder.
SecondaryComponents
¶ Returns the list of secondary components in the view
-------------------------------------
Getter Method
Signature
SecondaryComponents()
Returns: Return type: NXOpen.Drawings.DraftingComponentSelectionBuilder
New in version NX11.0.0.
License requirements: None.
Style¶
-
DetailViewBuilder.
Style
¶ Returns the style
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Drawings.ViewStyleBuilder
New in version NX6.0.0.
License requirements: None.
Type¶
-
DetailViewBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Drawings.DetailViewBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Drawings.DetailViewBuilderTypes
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
DetailViewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.