DraftingComponentSelectionBuilder Class¶
-
class
NXOpen.Drawings.
DraftingComponentSelectionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This builder allows the user to select a view in which component objects can be designated as primary or secondary geometry
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ObjectType | Returns or sets the object type |
Objects | Returns the selected objects (part occurrences) based on current object type |
Part | Returns or sets the part to use for populating the primary and secondary components object list |
PartForKF | Returns the part to use for populating the primary and secondary components object list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ClearSecondaryComponentList | Clears the secondary component list. |
InitializeListFromObject | Initialize list of components from the input object’s components list. |
ResetListToGlobal | Reset list of components to those specified by Properties->Drawings->Secondary Geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DraftingComponentSelectionBuilderGeometry Enumeration | type of geometry |
Property Detail¶
ObjectType¶
-
DraftingComponentSelectionBuilder.
ObjectType
¶ Returns or sets the object type
-------------------------------------
Getter Method
Signature
ObjectType()
Returns: Return type: NXOpen.Drawings.DraftingComponentSelectionBuilderGeometry
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectType(objectType)
Parameters: objectType ( NXOpen.Drawings.DraftingComponentSelectionBuilderGeometry
) –New in version NX11.0.0.
License requirements: None.
Objects¶
-
DraftingComponentSelectionBuilder.
Objects
¶ Returns the selected objects (part occurrences) based on current object type
-------------------------------------
Getter Method
Signature
Objects()
Returns: list of part occurrences Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
Part¶
-
DraftingComponentSelectionBuilder.
Part
¶ Returns or sets the part to use for populating the primary and secondary components object list
-------------------------------------
Getter Method
Signature
Part()
Returns: Return type: NXOpen.Part
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Part(part)
Parameters: part ( NXOpen.Part
) –New in version NX11.0.0.
License requirements: None.
PartForKF¶
-
DraftingComponentSelectionBuilder.
PartForKF
¶ Returns the part to use for populating the primary and secondary components object list
-------------------------------------
Getter Method
Signature
PartForKF()
Returns: Return type: NXOpen.Part
New in version NX11.0.0.
License requirements: None.
Method Detail¶
ClearSecondaryComponentList¶
-
DraftingComponentSelectionBuilder.
ClearSecondaryComponentList
¶ Clears the secondary component list.
Signature
ClearSecondaryComponentList()
New in version NX11.0.0.
License requirements: None.
InitializeListFromObject¶
-
DraftingComponentSelectionBuilder.
InitializeListFromObject
¶ Initialize list of components from the input object’s components list.
Signature
InitializeListFromObject(inputObject)
Parameters: inputObject ( NXOpen.NXObject
) –New in version NX11.0.0.
License requirements: None.
ResetListToGlobal¶
-
DraftingComponentSelectionBuilder.
ResetListToGlobal
¶ Reset list of components to those specified by Properties->Drawings->Secondary Geometry
Signature
ResetListToGlobal()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
DraftingComponentSelectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.