ViewScaleBuilder Class¶
-
class
NXOpen.Drawings.
ViewScaleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the View Scale (Drawings.
ViewScaleBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Denominator | Returns or sets the scale denominator |
Expression | Returns or sets the scale expression |
Numerator | Returns or sets the scale numerator |
ScaleType | Returns or sets the scale type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ViewScaleBuilderType Enumeration | The view scale type |
Property Detail¶
Denominator¶
-
ViewScaleBuilder.
Denominator
¶ Returns or sets the scale denominator
-------------------------------------
Getter Method
Signature
Denominator()
Returns: returns the denominator for the view’s scale Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Denominator(denominator)
Parameters: denominator (float) – sets the denominator for the view’s scale New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Expression¶
-
ViewScaleBuilder.
Expression
¶ Returns or sets the scale expression
-------------------------------------
Getter Method
Signature
Expression()
Returns: returns the expression used to determine the view scale. It will only be used if type is set to Drawings.ViewScaleBuilderType.Expression
.Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Expression(expression)
Parameters: expression ( NXOpen.Expression
) – sets the expression used to determine the view scale. It will only be used if type is set toDrawings.ViewScaleBuilderType.Expression
.New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Numerator¶
-
ViewScaleBuilder.
Numerator
¶ Returns or sets the scale numerator
-------------------------------------
Getter Method
Signature
Numerator()
Returns: returns the numerator for the view’s scale Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Numerator(numerator)
Parameters: numerator (float) – sets the numerator for the view’s scale New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ScaleType¶
-
ViewScaleBuilder.
ScaleType
¶ Returns or sets the scale type
-------------------------------------
Getter Method
Signature
ScaleType()
Returns: returns the scale type. Return type: NXOpen.Drawings.ViewScaleBuilderType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScaleType(type)
Parameters: type ( NXOpen.Drawings.ViewScaleBuilderType
) – sets the scale type.New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewScaleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.