DrawingSheetBuilderSheetStandardEnglishScale Enumeration

NXOpen.Drawings.DrawingSheetBuilder.SheetStandardEnglishScale is an alias for NXOpen.Drawings.DrawingSheetBuilderSheetStandardEnglishScale

class NXOpen.Drawings.DrawingSheetBuilderSheetStandardEnglishScale

Bases: object

the standard English drawing sheet scales

Enum Members

Enum Member Enum Member Description
S81
a scale of 8:1
S41
a scale of 4:1
S21
a scale of 2:1
S11
a scale of 1:1
S12
a scale of 1:2
S14
a scale of 1:4
S18
a scale of 1:8
Custom
a custom scale
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.