ViewBreakBuilder Class¶
-
class
NXOpen.Drawings.
ViewBreakBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.ViewBreakBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AddForeshorteningSymbol | Returns or sets the foreshortening symbol addition |
BreakGap | Returns or sets the break gap |
BreakLineAmplitude | Returns or sets the break line amplitude |
BreakLineColorWidth | Returns the break line color width |
BreakLineExtension | Returns or sets the break line extension |
BreakLineStyle | Returns or sets the break line style |
PropagateViewBreak | Returns or sets the propagate view break |
ShowBreakLines | Returns or sets the show break lines |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ViewBreakBuilderViewbreaklinestyle Enumeration | style for view break line |
Property Detail¶
AddForeshorteningSymbol¶
-
ViewBreakBuilder.
AddForeshorteningSymbol
¶ Returns or sets the foreshortening symbol addition
-------------------------------------
Getter Method
Signature
AddForeshorteningSymbol()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddForeshorteningSymbol(propagateViewBreak)
Parameters: propagateViewBreak (bool) – New in version NX11.0.0.
License requirements: drafting (“DRAFTING”)
BreakGap¶
-
ViewBreakBuilder.
BreakGap
¶ Returns or sets the break gap
-------------------------------------
Getter Method
Signature
BreakGap()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakGap(breakGap)
Parameters: breakGap (float) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
BreakLineAmplitude¶
-
ViewBreakBuilder.
BreakLineAmplitude
¶ Returns or sets the break line amplitude
-------------------------------------
Getter Method
Signature
BreakLineAmplitude()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakLineAmplitude(breakLineAmplitude)
Parameters: breakLineAmplitude (float) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
BreakLineColorWidth¶
-
ViewBreakBuilder.
BreakLineColorWidth
¶ Returns the break line color width
-------------------------------------
Getter Method
Signature
BreakLineColorWidth()
Returns: Return type: NXOpen.LineColorFontWidthBuilder
New in version NX9.0.0.
License requirements: None.
BreakLineExtension¶
-
ViewBreakBuilder.
BreakLineExtension
¶ Returns or sets the break line extension
-------------------------------------
Getter Method
Signature
BreakLineExtension()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakLineExtension(breakLineExtension)
Parameters: breakLineExtension (float) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
BreakLineStyle¶
-
ViewBreakBuilder.
BreakLineStyle
¶ Returns or sets the break line style
-------------------------------------
Getter Method
Signature
BreakLineStyle()
Returns: Return type: NXOpen.Drawings.ViewBreakBuilderViewbreaklinestyle
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakLineStyle(breakLineStyle)
Parameters: breakLineStyle ( NXOpen.Drawings.ViewBreakBuilderViewbreaklinestyle
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
PropagateViewBreak¶
-
ViewBreakBuilder.
PropagateViewBreak
¶ Returns or sets the propagate view break
-------------------------------------
Getter Method
Signature
PropagateViewBreak()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PropagateViewBreak(propagateViewBreak)
Parameters: propagateViewBreak (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
ShowBreakLines¶
-
ViewBreakBuilder.
ShowBreakLines
¶ Returns or sets the show break lines
-------------------------------------
Getter Method
Signature
ShowBreakLines()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowBreakLines(showBreakLines)
Parameters: showBreakLines (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewBreakBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.