VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsOverlayDataToUse Enumeration¶
NXOpen.Drawings.VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse is an alias for NXOpen.Drawings.VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsOverlayDataToUse
-
class
NXOpen.Drawings.
VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsOverlayDataToUse
¶ Bases:
object
Overlay Data To Use This indicate various options that can be used before Overlaying
Enum Members
Enum Member Enum Member Description AskatRuntime This option tells to show messages at rumtimeAlwaysUseExistingData This option will use existing data to overlayAlwaysCreateNewData This option will always create new dataCreateNewDataifNoneExists This option will create new data if none exists-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-