ProjectedViewOrientationBuilder Class

class NXOpen.Drawings.ProjectedViewOrientationBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Drawings.ProjectedViewOrientationBuilder

New in version NX9.0.0.

Properties

Property Description
NormalDirection Returns or sets the xform that represents the orthographic projected view settings to be edited
Tag Returns the Tag for this object.
XDirection Returns or sets the x direction vector for the orthographic projected view settings to be edited

Methods

Method Description
Restore Removes the associativity to the defined plane and x direction vector and restores the member view to its default orientation.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

NormalDirection

ProjectedViewOrientationBuilder.NormalDirection

Returns or sets the xform that represents the orthographic projected view settings to be edited

-------------------------------------

Getter Method

Signature NormalDirection()

Returns:
Return type:NXOpen.Xform

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NormalDirection(normalDirection)

Parameters:normalDirection (NXOpen.Xform) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

XDirection

ProjectedViewOrientationBuilder.XDirection

Returns or sets the x direction vector for the orthographic projected view settings to be edited

-------------------------------------

Getter Method

Signature XDirection()

Returns:
Return type:NXOpen.Direction

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XDirection(xDirection)

Parameters:xDirection (NXOpen.Direction) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Restore

ProjectedViewOrientationBuilder.Restore

Removes the associativity to the defined plane and x direction vector and restores the member view to its default orientation.

Signature Restore()

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Validate

ProjectedViewOrientationBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.