ShipbuildingLinesViewStyleLines Enumeration

NXOpen.Drawings.ShipbuildingLinesViewStyle.Lines is an alias for NXOpen.Drawings.ShipbuildingLinesViewStyleLines

class NXOpen.Drawings.ShipbuildingLinesViewStyleLines

Bases: object

Line type

Enum Members

Enum Member Enum Member Description
Hidden
Hidden
Visible
Visible
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.