DrawingFormatSheetBuilder Class

class NXOpen.Drawings.DrawingFormatSheetBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Drawings.DrawingFormatSheetBuilder

New in version NX9.0.0.

Properties

Property Description
InitialSecondarySheetNumber Returns or sets the initial secondary sheet number
InitialSheetNumber Returns or sets the initial sheet number
SecondaryNumberDelimiter Returns or sets the secondary number delimiter
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

InitialSecondarySheetNumber

DrawingFormatSheetBuilder.InitialSecondarySheetNumber

Returns or sets the initial secondary sheet number

-------------------------------------

Getter Method

Signature InitialSecondarySheetNumber()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature InitialSecondarySheetNumber(initialSecondarySheetNumber)

Parameters:initialSecondarySheetNumber (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

InitialSheetNumber

DrawingFormatSheetBuilder.InitialSheetNumber

Returns or sets the initial sheet number

-------------------------------------

Getter Method

Signature InitialSheetNumber()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature InitialSheetNumber(initialSheetNumber)

Parameters:initialSheetNumber (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

SecondaryNumberDelimiter

DrawingFormatSheetBuilder.SecondaryNumberDelimiter

Returns or sets the secondary number delimiter

-------------------------------------

Getter Method

Signature SecondaryNumberDelimiter()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SecondaryNumberDelimiter(secondaryNumberDelimiter)

Parameters:secondaryNumberDelimiter (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

DrawingFormatSheetBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.