ViewStyleSmoothEdgesBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleSmoothEdgesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the SMOOTH EDGES tab on the View Style Dialog (Drawings.
ViewStyleSmoothEdgesBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color on the SMOOTH EDGES tab of the View Style Dialog |
EndGaps | Returns or sets the end gaps toggle on the SMOOTH EDGES tab of the View Style Dialog |
EndGapsDistance | Returns or sets the end gaps data on the SMOOTH EDGES tab of the View Style Dialog |
Font | Returns or sets the font on the SMOOTH EDGES tab of the View Style Dialog |
SmoothEdge | Returns or sets the smooth edge toggle on the SMOOTH EDGES tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the angle tolerance toggle on the SMOOTH EDGES tab of the View Style Dialog |
ToleranceValue | Returns or sets the angle tolerance data on the SMOOTH EDGES tab of the View Style Dialog |
Width | Returns or sets the width on the SMOOTH EDGES tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Color¶
-
ViewStyleSmoothEdgesBuilder.
Color
¶ Returns or sets the color on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Color()
Returns: Returns the color that is on the smooth edges sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – Sets a new color on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
EndGaps¶
-
ViewStyleSmoothEdgesBuilder.
EndGaps
¶ Returns or sets the end gaps toggle on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
EndGaps()
Returns: Returns the end gaps toggle value that is on the smooth edges sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndGaps(endGapsToggle)
Parameters: endGapsToggle (bool) – Sets a new end gaps toggle value on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
EndGapsDistance¶
-
ViewStyleSmoothEdgesBuilder.
EndGapsDistance
¶ Returns or sets the end gaps data on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
EndGapsDistance()
Returns: Returns the end gaps data that is on the smooth edges sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndGapsDistance(endGapsData)
Parameters: endGapsData (float) – Sets new end gaps data on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Font¶
-
ViewStyleSmoothEdgesBuilder.
Font
¶ Returns or sets the font on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Font()
Returns: Returns the font that is on the smooth edges sub-builder Return type: NXOpen.Preferences.Font
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Font(font)
Parameters: font ( NXOpen.Preferences.Font
) – Sets a new font on the smooth edge sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SmoothEdge¶
-
ViewStyleSmoothEdgesBuilder.
SmoothEdge
¶ Returns or sets the smooth edge toggle on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
SmoothEdge()
Returns: Returns the smooth edge toggle value that is on the smooth edges sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothEdge(smoothEdgesToggle)
Parameters: smoothEdgesToggle (bool) – Sets a new smooth edge toggle value on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Tolerance¶
-
ViewStyleSmoothEdgesBuilder.
Tolerance
¶ Returns or sets the angle tolerance toggle on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Returns the tolerance toggle value that is on the smooth edges sub-builder Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(toleranceToggle)
Parameters: toleranceToggle (bool) – Sets a new tolerance toggle value on the smooth edge sub-builder New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
ToleranceValue¶
-
ViewStyleSmoothEdgesBuilder.
ToleranceValue
¶ Returns or sets the angle tolerance data on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ToleranceValue()
Returns: Returns the tolerance data that is on the smooth edges sub-builder Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceValue(toleranceData)
Parameters: toleranceData (float) – Sets new tolerance data on the smooth edge sub-builder New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Width¶
-
ViewStyleSmoothEdgesBuilder.
Width
¶ Returns or sets the width on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Width()
Returns: Returns the width that is on the smooth edges sub-builder Return type: NXOpen.Preferences.Width
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.Preferences.Width
) – Sets a new width on the smooth edge sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleSmoothEdgesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.