DraftingCurveInfoDraftingCurveType Enumeration¶
NXOpen.Drawings.DraftingCurveInfo.DraftingCurveType is an alias for NXOpen.Drawings.DraftingCurveInfoDraftingCurveType
-
class
NXOpen.Drawings.
DraftingCurveInfoDraftingCurveType
¶ Bases:
object
Specifies the drafting curve types
Enum Members
Enum Member Enum Member Description ExtractedEdge Specifies Extracted Edge CurveExtractedModelCurve Specifies Extracted Model CurveSilhouetteCurve Specifies Silhouette CurveThreadSilhouetteCurve Specifies Thread Silhouette CurveSectionEdge Specifies Section Edge CurveThreadSectionEdge Specifies Thread Section Edge CurveVICurve Specifies Virtual Intersection CurveUVHatchCurve Specifies UVHatch CurveTracelineCurve Specifies TraceLine CurveSimplifiedCurve Specifies Simplified CurveInterferenceCurve Specifies Interference Curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-