VisibleLinesViewStyle Class¶
-
class
NXOpen.Drawings.
VisibleLinesViewStyle
¶ Bases:
object
Represents set of Visible Lines View Style Preferences applicable to drafting views.
To obtain an instance of this class use
Drawings.ViewStyle.VisibleLines()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
VisibleColor | Returns or sets the visible color. |
VisibleFont | Returns or sets the visible font. |
VisibleWidth | Returns or sets the visible width. |
Methods¶
Property Detail¶
VisibleColor¶
-
VisibleLinesViewStyle.
VisibleColor
¶ Returns or sets the visible color.
The value should be between 1 and 216.
-------------------------------------
Getter Method
Signature
VisibleColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleColor(visibleColor)
Parameters: visibleColor (int) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
VisibleFont¶
-
VisibleLinesViewStyle.
VisibleFont
¶ Returns or sets the visible font.
-------------------------------------
Getter Method
Signature
VisibleFont()
Returns: Return type: NXOpen.Preferences.Font
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleFont(visibleFont)
Parameters: visibleFont ( NXOpen.Preferences.Font
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
VisibleWidth¶
-
VisibleLinesViewStyle.
VisibleWidth
¶ Returns or sets the visible width.
-------------------------------------
Getter Method
Signature
VisibleWidth()
Returns: Return type: NXOpen.Preferences.Width
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleWidth(visibleWidth)
Parameters: visibleWidth ( NXOpen.Preferences.Width
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)