ViewStyleFPCurvesBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleFPCurvesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Curve section of the Flat Pattern tab on the View Style Dialog (Drawings.
ViewStyleFPCurvesBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color on the Curve section of the Flat Pattern tab of the View Style Dialog |
Font | Returns or sets the font on the Curve section of the Flat Pattern tab of the View Style Dialog |
State | Returns or sets the state toggle on the Curve section of the Flat Pattern tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Type | Returns the type of Flat Pattern Curve |
Width | Returns or sets the width on the Curve section of the Flat Pattern tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Color¶
-
ViewStyleFPCurvesBuilder.
Color
¶ Returns or sets the color on the Curve section of the Flat Pattern tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Color()
Returns: Returns the color that is on the curve section of the flat pattern sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – Sets a new color on the curve section of the flat pattern sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Font¶
-
ViewStyleFPCurvesBuilder.
Font
¶ Returns or sets the font on the Curve section of the Flat Pattern tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Font()
Returns: Returns the font that is on the curve section of the flat pattern sub-builder Return type: NXOpen.Preferences.Font
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Font(font)
Parameters: font ( NXOpen.Preferences.Font
) – Sets a new font on the curve section of the flat pattern sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
State¶
-
ViewStyleFPCurvesBuilder.
State
¶ Returns or sets the state toggle on the Curve section of the Flat Pattern tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
State()
Returns: Returns the state toggle value that is on the curve section of the flat pattern sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
State(stateToggle)
Parameters: stateToggle (bool) – Sets a new state toggle value on the curve section of the flat pattern sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Type¶
-
ViewStyleFPCurvesBuilder.
Type
¶ Returns the type of Flat Pattern Curve
-------------------------------------
Getter Method
Signature
Type()
Returns: Returns the type of flat pattern curve Return type: NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectType
New in version NX6.0.0.
License requirements: None.
Width¶
-
ViewStyleFPCurvesBuilder.
Width
¶ Returns or sets the width on the Curve section of the Flat Pattern tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Width()
Returns: Returns the width that is on the curve section of the flat pattern sub-builder Return type: NXOpen.Preferences.Width
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.Preferences.Width
) – Sets a new width on the curve section of the flat pattern sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleFPCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.