FlatPatternSettingsFlatPatternObjectType Enumeration

NXOpen.SheetMetal.FlatPatternSettings.FlatPatternObjectType is an alias for NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectType

class NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectType

Bases: object

The members of the following enumerated type are used to identify object types to the FlatPatternView API.

These are not the usual NX object types; they are ordinary NX objects that are known to the flat pattern feature for the type of outline they provide to a bend region, joggle region, or lightening hole.

Enum Members

Enum Member Enum Member Description
BendCenterLine
Deprecated
BendUpCenterLine
BendDownCenterLine
BendTangentLine
OuterMoldLine
InnerMoldLine
ExteriorCurves
InteriorCurves
Deprecated
InteriorCutoutCurves
InteriorFeatureCurves
LighteningHoleCenter
JoggleLine
AddedTopGeometry
AddedBottomGeometry
ToolMarker
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.